Bayer Demosaicing For Bilinear Line Scan Cameras with Color Pattern RedFollowedByBlue GreenFollowedByGreen

Brief Description

File: \examples\Processing\Color\Bayer\BilinearBayer_RB_GG.va

Default Platform: mE5-MA-VCL

Short Description

The example shows the demosaicing of a Bayer RAW pattern of a bilinear line scan camera with color pattern Red/BlueFollowedBlue/Red_GreenFollowedGreen in "DeBayer Enhanced" and "DeBayer Fast" (is "Bayer Raw") mode.

In the VisualApplets design example "BilinearBayer_RB_GG.va" the Bayer demosaicing for a bilinear line scan camera with colors red followed by blue or vice versa in the first sensor (top) line and colors green in the second (bottom) sensor line (or vice versa) is implemented. See Fig. 257 for the visualization of the sensor layout.

Sensor layout of a bilinear line scan camera with color pattern Red/BlueFollowedByBlue/Red_GreenFollowedByGreen

Figure 257. Sensor layout of a bilinear line scan camera with color pattern Red/BlueFollowedByBlue/Red_GreenFollowedByGreen


The Bayer demosaicing for this sensor layout is implemented in the applet for two camera modes: the "DeBayer Fast" mode and the "DeBayer Enhanced" mode. In the first case the motion between two acquisitions is two sensor lines, in the second case one line. Due to this, one color component is acquired for each pixel in the "DeBayer Fast" mode and two color components (red and green or blue and green) per pixel in the "DeBayer Enhanced" mode. In Fig. 258 you can see the basic structure of the design "BilinearBayer_RB_GG.va".

Basic design structure of "BilinearBayer_RB_GG.va"

Figure 258. Basic design structure of "BilinearBayer_RB_GG.va"


An image acquired in "DeBayer Fast" or "DeBayer Enhanced" mode by a bilinear line scan camera in Camera Link Full configuration (see camera interface operator FullGrayCamera) is demosaiced in the HierarchicalBox DeBayer. With "right-mouse-click" on this box you can choose the Bayer pattern and the white balancing coefficients for red, green and blue under "Properties". The fully color interpolated rgb image is transmitted to PC via DMA. The default platform for this design is microEnable 5 marathon VCL, but it can easily be adapted to another platform. For the design you can find test images for the "DeBayer Enhanced" mode and the "DeBayer Fast" mode under \examples\Processing\Color\Bayer\TestImagesBilinearBayer. The content of box DeBayer is shown in Fig. 259.

Content of HierarchicalBox DeBayer

Figure 259. Content of HierarchicalBox DeBayer


In the HierarchicalBox WhiteBalance a white balancing of the red, green and blue components is performed. You can choose the white balancing coefficients directly with "double-mouse-click" on the operator WhiteBalanceBayer in this box or with "right-mouse-click" on the box "DeBayer" as described above. The operator FIRkernelNxM_Kernel5x5 creates a 5x5 pixel kernel around the current pixel. With the operator SourceSelector_SelectFast you can choose the DeBayer mode DeBayerEnhanced or DeBayerFast. In Fig. 260 you can see the content of box DeBayerEnhanced.

Content of HierarchicalBox DeBayerEnhanced

Figure 260. Content of HierarchicalBox DeBayerEnhanced


From the 5x5 kernel, a 3x2 sub kernel is selected. In the first row the red and blue values and in the second the green color values (or vice versa) are located. See for visualization of the kernel components order Fig. 261 for an example Bayer pattern of "RedFollowedByBlue_GreenFollowedByGreen".

Kernel components selected in HierarchicalBox DeBayerEnhanced by operator SelectSubKernel3x2

Figure 261. Kernel components selected in HierarchicalBox DeBayerEnhanced by operator SelectSubKernel3x2


With the operator combination SelectSubKernel-FirstPixel, ModuloCountLine and RemoveLine redundant image lines are removed. (The line redundancy occurs from the kernel creation.) With the operators SelectSubKernel-BR and SelectSubKernel-G the red and blue kernel components are separated from the green kernel components. If the Bayer pattern has the green values in the first kernel row, the components can be swapped in the HierarchicalBox Swap with the constant IsBRthenGG. The constant is set automatically, if you have chosen the Bayer pattern with "right-mouse-click" on the box "DeBayer" as described above. In the box Interpolation the missing third color component red () or blue () at pixel position is interpolated according to:

Equation 14.


其中 are the green color components at pixel position . The color components are finally merged together with the operator MergeComponents.

If you choose the "Bayer Raw" (also called "DeBayer Fast") mode of your camera, for each pixel only one color is acquired, due to the doubled line speed in comparison to the method described above. For this camera mode you can choose for DeBayering of the color components box DeBayerFast (see Fig. 259). You can see the content of box DeBayerFast in Fig. 262.

Content of HierarchicalBox DeBayerFast

Figure 262. Content of HierarchicalBox DeBayerFast


Here the DeBayering of the color components red , blue or green at pixel position is performed in the following way. The red or blue color components on a blue or red pixel are interpolated according to:

Equation 15.


The green color components on a red or blue pixel are interpolated according to:

Equation 16.


The red or blue color components on a green pixel in a red or blue pixel column can be calculated as:

Equation 17.


Finally the red or blue color components on green pixel in a blue or red pixel column are evaluated as:

Equation 18.


For each pixel the evaluated red, green and blue color components are merged together with the operator MergeComponents (see Fig. 262) The complete image is finally transmitted via DMA to PC as shown in the basic design structure in Fig. 258.